There is a table in the Operating Manual with wire sizes based on current. See http://literature.cdn.keysight.com/litweb/pdf/N8900-90901.pdf#page=36.
However, you also need to make sure the wires insulation rating is high enough for the unit it is being use with. Typical wires only have a voltage rating of between 300 to 600V.
Applies to: N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8937APV, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A, N8957APV
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |